Two Cooling fan P/N in the LS1046A RDB board where using?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two Cooling fan P/N in the LS1046A RDB board where using?

ソリューションへジャンプ
1,755件の閲覧回数
michael_lee1
Contributor I

#LS1046A RDB,#BOM LS1046A,#ventilation fan P/N,cooling fan P/N

タグ(1)
0 件の賞賛
1 解決策
1,456件の閲覧回数
ufedor
NXP Employee
NXP Employee

The provided data sheet is for the chassis fans.

元の投稿で解決策を見る

7 返答(返信)
1,456件の閲覧回数
michael_lee1
Contributor I

The RDB P/N is LS1046ARDB-PB.

Pls, check it over the document where the picture shown.

Ths,

0 件の賞賛
1,456件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please see the fan data sheet attached.

0 件の賞賛
1,456件の閲覧回数
michael_lee1
Contributor I

Hi Ufedor,

 

Thanks a lot for the information.

Is it the same cooling fan using in the board where LS1046A processor cooling fan and other 2 side ventilation fans are same one, as provided P/N?

Thanks,

0 件の賞賛
1,457件の閲覧回数
ufedor
NXP Employee
NXP Employee

The provided data sheet is for the chassis fans.

1,456件の閲覧回数
michael_lee1
Contributor I

Thanks for the answer.

Can I have the information of the cooling fan P/N of the LS1046A in the top?

Pls, provided me the detail info and full P/N as well.

Regards,

0 件の賞賛
1,456件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no such fan on the LS1046ARDB-PB:

2019-01-21_160413.jpg

0 件の賞賛
1,456件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which exactly RDB revision is in question?

Please provide a clear photo of the on-the-case stickers.

0 件の賞賛