Hi,
I tried downloading both SDK 0.4 and SDK 0.5 from NXP website, SDK 0.4 does not have default config and policy files for FMC tool, whereas SDK 0.5 has config and policy files under etc/fmc/config/private/<board name >/<RCW>/config.xml and policy_ipv4.xml.
Is this files not required in SDK 0.4 version ?
Thanks,
Manjunath
SDK 0.4 is missing a package that provides pre-built FMC confguration files, eth-config. DPAA kernel driver starts with some workable queue configuration without FMC invocation from the userland, so basic connectivity will work under rev 0.4. If, however, you are to work with a custom FMAN configuration under 0.4, create both files by hand, bring them from NXP git (sdk/eth-config.git - Ethernet configuration ), or better, move to SDK 0.5.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Platon,
Thanks for suggestion, will try getting eth-config from NXP git.
I had initially tried SDK 0.5 but faced issues, not able to ping, FMC crashes. Both issues i have posted here but no solution.
https://community.freescale.com/message/629960?et=watches.email.thread#comment-629960
Thanks,
Manjunath