We are using P1012(QorIQ) on product board.
There is a problem that the core 1V power supply is rarely short-circuited in P1012,
when power supply to P1012 is started.
In Chapter 2.5 on P1012 hardware specification (P1012EC.pdf),
we have the following description.
1) Controlling the maximum power-on ramp rate is required to avoid falsely triggering the ESD circuitry.
2) If non-linear (for example. exponential), the maximum rate of change from 200 to 500 mV
is the most critical as this range might falsely trigger the ESD circuitry.
If we do not observe this description and start up the 1 V power supply,
does the 1V power supply short in the P1012 ?
Yes, if this requirement is not met, than internal ESD protection circuits may be triggered. Triggering these circuits mean opening a direct current path to ground to protect all other circuit from high voltage.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------