The root file system extracted from the QorIQ SDK V2.0-1703 supplied images does not have root account and environment configured.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The root file system extracted from the QorIQ SDK V2.0-1703 supplied images does not have root account and environment configured.

386 次查看
stephenmcintyre
Contributor II

I created a boot SD card and loaded the rootfs as described in the SDK document section SD deployment 4.4.16.9.4 Item 6. Copy the file system to harddisk by extracing the QorIQ_SDK_<Version>_E6500_<release
date>_ROOTFS_Image.tar.gz. Remove the tarball after extracting rootfs.
# cp QorIQ_SDK_<Version>_E6500_<release date>_ROOTFS_Image.tar.gz
# sudo tar -zxvf QorIQ_SDK_<Version>_E6500_<release date>_ROOTFS_Image.tar.gz
# rm QorIQ_SDK_<Version>_E6500_<release date>_ROOTFS_Image.tar.gz

specifically I installed using this file QorIQ_SDK_V2.0_E5500_64B_20160527_ROOTFS_Image.tar.gz

Which works, but the file system does not include the root account and or the environment configured. Is there a script file available or do I have to create the root account environment myself? or am I just missing something?

I thought that this tarball would have recreated the basic file system as supplied on our devkit.

标记 (2)
0 项奖励
0 回复数