The problem of LS1088A I2C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem of LS1088A I2C

728 Views
NaihuaZhang
Contributor I

From the LS1088A chip Errata,the A-010650 shows the problem of I2C  controller,and advieces that use an open drain GPIO pin to connect the I2Cx_SCL.

For I2C1 and I2C2,I use GPIO3_07、GPIO3_11 to connect the I2C1_SCL and I2C2_SCL.

But for I2C3 and I2C4, I see I2C3_SCL and I2C4_SCL can be configured as open GPIO by performing hardware modification, so I don’t use extra GPIO to connect them. Is this usage correct?

0 Kudos
Reply
0 Replies