TDM interface is critical to our product in mind since the chipsets that we intend to use are giving PCM output
Questions -
Will the TDM interface for 1043 series processor be able to take in PCM input directly or it needs something in between?
There was a mention of TDM riser card in the documentation, is that an optional component?
Does the evaluation toolkit come with some tool which can help us generate PCM data and drive the TDM interfaces of the processor for the time being ?
Thanks
Ajay
>Will the TDM interface for 1043 series processor be able to take in PCM input directly or it needs something in between?
>
[Platon] It depends on the frame structure, timing and signal voltage levels of your TDM peripheral. Refer to
QEIWRM Chapter 22, LS1043ARM Section 14.3.11, LS1043A Datasheet Section 3.11.2.
>There was a mention of TDM riser card in the documentation, is that an optional component
>
[Platon] Yes, it is optional.
>Does the evaluation toolkit come with some tool which can help us generate PCM data and drive the TDM interfaces
>of the processor for the time being ?
>
[Platon] There are no specific configuration or data generation tools. The SDK for LS1043ARDB includes a compact TDM driver
for minimum interface testing. Details can be found in the SDK Release Notes, Chapter 32.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------