T2081 COP CONNECTION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2081 COP CONNECTION

571 Views
hemanttiwari199
Contributor III

Hi,

How can I make the connection for JTAG/COP port for T2081 ? Please note that I am not using CPLD in my design.

Any help will be appreciated.

Regards

Hemant

0 Kudos
3 Replies

553 Views
r8070z
NXP Employee
NXP Employee

Unfortunately, I cannot recommend any third party devices. I think you can use “Power Supply Monitor with Reset” device of any manufacturer. Just as example see MAX6335.

0 Kudos

566 Views
r8070z
NXP Employee
NXP Employee

Please see JTAG/COP port implementation in section "JTAG system-level recommendations" of the QorIQ T2080 Design Checklist
https://www.nxp.com/docs/en/application-note/AN4804.pdf

0 Kudos

561 Views
hemanttiwari199
Contributor III

Hi,

Thanks for the reply.

Can you please suggest/recommend me the logic gate part number to be used to implement the cop_trst_b and poreset_b?

Regards

Hemant

0 Kudos