T2081 10G Ethernet problems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2081 10G Ethernet problems

1,105 次查看
gyosunshim
Contributor III

Hi All,

 

T2080RDB EVM board using the design was similar to the T2081 board.

10G PHY (CS4315) related circuit configuration is the same.

uboot was modified to change the SRDS_PRCTL_S1 value from 0x66 to 0x6C.

However, T2081 10G Ethernet board is recognized even seems never.

 

It was attached to the boot log file.

Is there should be more information to be corrected in uboot code?

What's wrong? I need help.

 

Best regards,

gyosun.

Original Attachment has been moved to: fail_bd2.log.zip

0 项奖励
回复
1 回复

933 次查看
bpe
NXP Employee
NXP Employee

Based on the log you attached, your 10G interfaces are recognized:

>sl_mac: fsl_mac: FSL FMan MAC API based driver ()

>...

>fsl_mac ffe4f0000.ethernet: FMan MEMAC

>fsl_mac ffe4f0000.ethernet: FMan MAC address: 00:04:9f:03:6a:7f

>fsl_mac ffe4f2000.ethernet: FMan MEMAC

>fsl_mac ffe4f2000.ethernet: FMan MAC address: 00:04:9f:03:6a:80

>...

What exactly is the problem?


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复