T2080 spi boot failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 spi boot failed

1,033 Views
liguofa
Contributor III

T2080 spi boot error, can not start, we can use the oscilloscope to see that rcw has been loaded. Where can I find the patch for u-boot-2016.01_bsp14.0? We are using the 1.1 version of the chip.PBI Command For T2080 I2C EEPROM Boot‌   @ufedor 

Our picture is as follows

pastedImage_1.png

Tags (2)
0 Kudos
Reply
2 Replies

937 Views
liguofa
Contributor III

I have solve the problem, cause clock of Serdes.

0 Kudos
Reply

937 Views
ufedor
NXP Employee
NXP Employee

> Where can I find the patch for u-boot-2016.01_bsp14.0?

Excuse me, what do you mean?

Are you still have issue with SPD EEPROM?

0 Kudos
Reply