T2080 custom board U-Boot booting issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 custom board U-Boot booting issue

2,396 次查看
ammasikaniv
Contributor II

Hi,

We are working with T2080RDB based custom board. 

It boots from NOR Flash. UBoot booting often crashes, but sometimes succeeds with few exceptions in between booting. Please find the attached file for the UBoot failure logs.

Can somebody help us to figure out the reason for UBoot crashing?

 

Below are NOR Flash and clock details used on the board:
- 256MB NOR flash (PC28F00BM29EWHA)
- DDR3L and System Reference clock 66.66 MHz

 

Below details are for attached logs
- U-boot booting log on second revision board for failure scenario
- U-boot booting log on second revision board for success scenario
- RCW values

 

Original Attachment has been moved to: U_boot_log_success.txt.zip

Original Attachment has been moved to: U-boot_log_Failure.txt.zip

Original Attachment has been moved to: RCW_Values.txt.zip

0 项奖励
回复
8 回复数

1,973 次查看
tapyang
Contributor III

Hi,

When an empty custom board comes, need I only burn RCW and Uboot?

What about the flash map address for your board?

I burn the RCW(e8000000) and Uboot(eff40000), and have no print in console...

Expect for your reply,  and Thank you very much.

0 项奖励
回复

1,973 次查看
ufedor
NXP Employee
NXP Employee

> I burn the RCW(e8000000) and Uboot(eff40000)

Which tool you've used and which board initialization file?

Is the NOR Flash size 256 MB?

0 项奖励
回复

1,973 次查看
tapyang
Contributor III

Hi, Dear ufedor:

I used codewarrior 10.5.1 and the initialization file is "T2080RDB-PCIe_init_core.tcl".

My Nor Flash size is 128MB.

And I debuged the UBOOT, it says "0xfffffffc is empty string"....

Expect for your reply,  and Thank you very much. Wish you a nice day.

0 项奖励
回复

1,973 次查看
ufedor
NXP Employee
NXP Employee

In the original wording it is written:

> Below are NOR Flash and clock details used on the board:
> - 256MB NOR flash (PC28F00BM29EWHA)

Now you wrote:

> My Nor Flash size is 128MB.

Which is wrong?

It is needed to inspect the processor connection schematics.

This can be conveniently done if you create a Technical Case:

https://community.nxp.com/thread/381898

0 项奖励
回复

1,973 次查看
tapyang
Contributor III

eh....,Sorry, I am another one, and My board's flash size is 128MB.

0 项奖励
回复

1,973 次查看
ufedor
NXP Employee
NXP Employee

Please create a Technical Case:

https://community.nxp.com/thread/381898

0 项奖励
回复

1,973 次查看
tapyang
Contributor III

OK

0 项奖励
回复

1,973 次查看
ufedor
NXP Employee
NXP Employee

Use a debugger, connect to the board in case of success and failure and dump DDR controller registers values.

0 项奖励
回复