T2080 - SERDES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 - SERDES

1,040 Views
manikumar
Contributor II

Hi,

Can SERDES 1 and 2 be configured independently. Or it should be configured as per combinations shown in below table?

pastedImage_2.png

As per RCW bits, its intimated that SRDS_PRTCL_S1 and SRDS_PRTCL_S2 be used in conjunction. But there were no details whether (Table 4-40 of T2080RM) combinations provided in Table 19-1 to be maintained. Please check and let me know.

Regards,

Mani

3 Replies

867 Views
Bulat
NXP Employee
NXP Employee

As mentioned in the manual, SRDS_PRTCL_S1 and SRDS_PRTCL_S2 are used in conjunction. Table 19-1 provides enabled combinations of those fields. The combination includes SRDS_PRTCL_S1 and SRDS_PRTCL_S2 values at the same row of the table. In your example these can be either 0x1C and 0x1F or 0x95 and 0x1F.

867 Views
manikumar
Contributor II

Hello Bulat,

Thanks for your reply,

As SERDES 1 and SERDES 2 are operated independently with REFCLK1 and REFCLK2. I am expecting that by using SRDS_PRTCL_S* registers they can configure independently.

Please let me know the requirement of using these combinations as per table 19-1.

Regards,

Mani

0 Kudos

867 Views
Bulat
NXP Employee
NXP Employee

I am not sure what you mean with "requirement of using". Can you clarify?

0 Kudos