T2080 :PCIe Data rate(5&2.5Gbps)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 :PCIe Data rate(5&2.5Gbps)

757 Views
anandram
Contributor I

Hi,
    I am using T2080 Processor in my custom board.
Our customer requirement is three x1 PCIe at 5Gbps data rate and one x1 PCIe at 2.5Gbps.

My serdes section hardware connections are as below.
Serdes-1 -->(x1 PCIe ,A), (x1 PCIe,E),(x1 PCIe,F),(x1 PCIe ,G)
Serdes-2 -->x2 AURORA (E,F)
The protocol i have chosen F8-36.
Is it possible to run 3  x1 PCIe lane at 5Gbps & one x1 PCIe lane at 2.5Gbps.

Please confirm.

Tags (1)
0 Kudos
3 Replies

507 Views
anandram
Contributor I

Hi NXP,

Can we use aurora in T2080 for high speed communication like PCIe? As per the reference manual, T2080 supports Aurora only for Real-time debugging with Lauterbach TRACE32.

Also I couldn't able to fetch any detail about aurora memory map registers in the QorIQ T2080 Reference Manual.

Please clarify.

0 Kudos

507 Views
ufedor
NXP Employee
NXP Employee

Aurora can be used as debug interface only and its detailed description is available only for debug tools vendors..

0 Kudos

507 Views
ufedor
NXP Employee
NXP Employee

> Is it possible to run 3  x1 PCIe lane at 5Gbps & one x1 PCIe lane at 2.5Gbps.

For the selected SerDes protocols (F8-36) maximum rate of all the PCIe controllers is determined by the SRDS_DIV_PEX_S1 - i.e. all four x1 PCIe lanes will have the same limit - 5Gbps.

0 Kudos