T1042NXE7MQB boot at Cold Temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042NXE7MQB boot at Cold Temperature

1,853 Views
kangquan
Contributor I

In our design, the T1042(with heat sink on the top of T1042) doesn't boot up at -20C when we turn on the cooling fans, if we turn off the fans, the T1042(with heat sink on the top of T1042) doesn't boot up at -35C, if we take off the heat sink and turn off the fans, the T1042 doesn't have boot up issue, it can boot up at -40C

We already checked the input system clock(DIFF_SYSCLK/DIFF_SYSCLK_B) at -40C, it looks like the same at room temperature. When T1042 doesn't boot up, PORESET_B and RESET_REQ_B both are HIGH, but HRESET_B is LOW, all the voltages level are look good. We tested the 1042 can boot up or cannot boot up by itself as temperature up and down without turn off the power. We even tested the hard-coded RCW setting, the T1042 doesn't boot up at cold temperature.

So I am just wondering if the T1042 has certain temperature protection when temperature reach to certain degree during power up?

0 Kudos
Reply
2 Replies

1,743 Views
kangquan
Contributor I

this problem has been fixed

0 Kudos
Reply

1,564 Views
wangyf
Contributor II

Hello kangquang, 

I have met the same issue as you, could you tell me how you solved the problem ?

Thanks very much, 

wangyf

0 Kudos
Reply