T1042D4RDB networking problems when booting from SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042D4RDB networking problems when booting from SD card

Jump to solution
5,583 Views
oyvind_harboe
Contributor I

I'm having problems with getting ethernet to work with T1042D4RDB when I'm booting from an SD Card.

Here's the output when I boot:

SERDES Reference : 0x86
Net: Initializing Fman

MMC read: dev # 0, block # 2080, count 128 ...
Fman1: Data at 7fdf8f88 is not a firmware
No ethernet found.
Hit any key to stop autoboot: 0
=> md 0x7df8f88
07df8f88: deadbeef deadbeef deadbeef deadbeef ................
07df8f98: deadbeef deadbeef deadbeef deadbeef ................
07df8fa8: deadbeef deadbeef deadbeef deadbeef ................
07df8fb8: deadbeef deadbeef deadbeef deadbeef ................
07df8fc8: deadbeef deadbeef deadbeef deadbeef ................
07df8fd8: deadbeef deadbeef deadbeef deadbeef ................
07df8fe8: deadbeef deadbeef deadbeef deadbeef ................   

From the u-boot code, we I can see that u-boot thought it was able to read from the SD card, but "0xdeadbeef" is indicative that nothing was written to RAM at that address.

Oddly, the return value from blk_dread() is not checked below in u-boot drivers/net/fm/fm.c:

   printf("\nMMC read: dev # %u, block # %u, count %u ...\n",
dev, blk, cnt);
  mmc_init(mmc);
  (void)blk_dread(mmc_get_blk_desc(mmc), blk, cnt,
addr);
}
[deleted]

/* Upload the Fman microcode if it's present */
rc = fman_upload_firmware(index, &reg->fm_imem, addr);
if (rc)
   return rc;
env_set_addr("fman_ucode", addr);

0 Kudos
Reply
1 Solution
5,437 Views
ufedor
NXP Employee
NXP Employee

It is needed to write FMan microcode (attached) to the SD card from block 0x820.

In U-Boot: =>tftp 100000 fsl_fman_ucode_t1040_r1.1_107_4_2.bin  =>mmc write 100000 820 37   In Linux: # dd if=fsl_fman_ucode_t1040_r1.1_107_4_2.bin of=/dev/sdb  seek=2080 bs=512

View solution in original post

0 Kudos
Reply
8 Replies
2,763 Views
motej40398
Contributor I

Wingstop.com/survey – Mywingstopsurvey.com/usa is an online survey offered by Wingstop, allowing customers to provide valuable feedback on their last visit experience.

The Wingstop company would like you to provide feedback to help them understand what can be changed to ensure customers an improved experience.

0 Kudos
Reply
3,609 Views
legikir105
Contributor I

Welcome to the Wendy's Customer Satisfaction Survey. We value your candid feedback and appreciate you taking the time to complete our survey.

https://haioly-tsiiv-splieurk.yolasite.com/

0 Kudos
Reply
3,483 Views
metewe1644
Contributor I

A login gateway designed just for Lockheed Martin workers is called LMPeople External. Employees can access a range of services through the portal, including pay stubs, benefits, and personal data.

 

0 Kudos
Reply
5,437 Views
oyvind_harboe
Contributor I

Clearification: this is not for Rasperry PI nor my PC, it's for T1042D4RDB.

0 Kudos
Reply
5,437 Views
oyvind_harboe
Contributor I

I see! Thanks! I didn't realize the fMan firmware wasn't included in the u-boot image.

I tried with 108.5.9, but it didn't work. T1042D4RDB ships with 106.4.18 and it worked.

I find it curious that 108.15.9 is included when it doesn't work and that you recommend 107.4.2. 

How did you arrive at the conclusion that 107.4.2 is the right version to program?

$ ls tmp/deploy/images/t1042d4rdb/fsl_*.bin
tmp/deploy/images/t1042d4rdb/fsl_fman_ucode_t1040_r1.1_106_4_18.bin
tmp/deploy/images/t1042d4rdb/fsl_fman_ucode_t1040_r1.1_107_4_2.bin
tmp/deploy/images/t1042d4rdb/fsl_fman_ucode_t1040_r1.1_108_5_9.bin

0 Kudos
Reply
5,437 Views
ufedor
NXP Employee
NXP Employee

FMan microcode revision has to be consistent with the SDK revision.

My assumption was that SDK v2.0 is used.

0 Kudos
Reply
5,437 Views
oyvind_harboe
Contributor I

I'm not using SDK v2.0. It's quite old and not compatible with Ubuntu 18, when I tried(Python 2 vs. 3 problems, near as I can tell).


I'm using Poky 2.6.1

Questions:

1. Why would Poky 2.6.1 ship with 3 different versions?

2. Why ship with the latest one that doesn't work?


Cheers,

0 Kudos
Reply
5,438 Views
ufedor
NXP Employee
NXP Employee

It is needed to write FMan microcode (attached) to the SD card from block 0x820.

In U-Boot: =>tftp 100000 fsl_fman_ucode_t1040_r1.1_107_4_2.bin  =>mmc write 100000 820 37   In Linux: # dd if=fsl_fman_ucode_t1040_r1.1_107_4_2.bin of=/dev/sdb  seek=2080 bs=512
0 Kudos
Reply