T1042 NOR FLASH Latch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1042 NOR FLASH Latch

1,743 次查看
yusufalti4444
Contributor I

Hello nxp experts,

In attached image, which shows 'Figure 24-9. Connection of x16 NOR for ADM MODE 0'. We want to cover Latch with an FPGA. FPGA will do same things as exactly like if there is no FPGA. We want to use FPGA because of some voltage problems. Pins will be connected as they used to be.

Our question is;

Latch requires 1 more cycle to perform his complete task. FPGA also requires one more cycle. When we add FPGA to system, Total required cycle to write NOR flash is going to be increased from 2 to 3. (1 cycle FPGA, 1 cycle latch, 1 cycle is default) (3 cycle for latch muxing inside FPGA, 2 cyle without latch mux, only fpga).

Can this system (FPGA added) works without any problem ? If it is, what procedure should we follow to change 'IFC flash timing registers' ?

I also wonder that how this 'IP Clock' is generated inside IFC ?

0 项奖励
回复
3 回复数

1,641 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

requires one more cycle

One more cycle of which frequency?

I also wonder that how this 'IP Clock' is generated inside IFC ?

The ip clock is not generated inside the IFC.

0 项奖励
回复

1,641 次查看
yusufalti4444
Contributor I

Hello,

>One more cycle of which frequency?

100MHZ

0 项奖励
回复

1,641 次查看
ufedor
NXP Employee
NXP Employee

Please consider that NOR Flash is a slow device, so implementing address latch on FPGA is a viable solution.

0 项奖励
回复