T1040RDK Ethernet Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040RDK Ethernet Driver

534 Views
kmanjushree
Contributor I

Hi

      I need to develop Ethernet driver software in C programming for T1040RDK. Can I get some sample source code either in C or Linux which can be used as a base for my development.

0 Kudos
Reply
1 Reply

456 Views
Pavel
NXP Employee
NXP Employee

Look at attached file. This file contains Ethernet driver from u-boot from NXP SDK 2.0 for the T1040RDB board.

 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply