T1040 16-Bit NVSRAM IFC Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1040 16-Bit NVSRAM IFC Configuration

872 Views
daveclark
Contributor I

I am having trouble mapping a 128KB NVRAM device into the IFC (GPCM mode) on a t1040.  The NVRAM device is a 1Mb (64Kx16) device and is the CY14V101NA.  The problem I am seeing is the first 64KB is being repeated, i.e. writing to offset 0 also writes to offset 0x10000.

We are using a custom vxWorks BSP which configures the IFC as follows:

CSOR2  0x00000000

AMASK2  0xFFFE0000

CSPR2_EXT  0xF

CSPR2  0xFFDE0085

LAWBARH3  0x0F

LAWBARL3  0xFFDE0000

LAWAR3  0x81F00010

I have tried changing the CSPR2 register to 0xFFDE0105 to enable x16 mode, but still see the same problem.

The device is connected as follows:

IFC_ADDR[31] - A0

    :             :

IFC_ADDR[16] - A15

IFC_AD[15] - DQ0

    :             :

IFC_AD[0] - DQ15

with BHE and BLE pulled low.

So my question is what have I missed?

Tags (4)
0 Kudos
2 Replies

685 Views
Bulat
NXP Employee
NXP Employee

Unfortunately you made a mistake with address connection. Note, the write to offset 0x10000 assumes that IFC_ADDR[15] is '1', other address bits are '0'. However in your scheme IFC_ADDR[15] is not even connected to the SRAM... This is why the SRAM does not see any difference between offsets 0x10000 and 0x00000.

Correct wiring for x16 bit memory should be as following:

IFC_ADDR[30] - A0

IFC_ADDR[29] - A1

    :             :

IFC_ADDR[15] - A15

Regards,

Bulat

685 Views
daveclark
Contributor I

Thanks for your reply, I suspected it was something like this, I was just hoping there was a solution that could be done from within the software. I'll speak to the hardware engineers next time I see them

0 Kudos