T1024RDB EEPROM Access

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1024RDB EEPROM Access

2,395 次查看
valentinmovsik
Contributor I

Hi Everyone,

I’m trying to find how to access(R/W) from Uboot to EEPROM on T1024RDB – AT24C256 (ADDR =0x50). I couldn’t find any explanation about it.

I found something in “QorIQ-SDK-2.0-IC-Rev0.pdf” p.95:

 

Writing SPD

DDRC takes its configuration parameters from EEPROM that are on I2C bus. To provide configuration to DDRC, its respective

EEPROM needs to be programmed with the desired configuration.

EEPROM for DDRC1 is at address 0x51

B4420QDS has only one DDRC, so only one SPD needs to be programmed for this DDR controller.

By default, EEPROMs are write protected. Use the following commands to make them writable:

mw.b 0xffdf0055 0x8

In order to write SPD, TFTP SPD binaries and write them on EEPROMs using the following commands:

tftp 1000000 spd_1866_dual_rank_4GB_DDRC1.bin

i2c write 0x1000000 0x51 0 0x80

reset

After configuring EEPROM, reset board to let DDRC settings take effect.

 

But all this above is only about B4420QDS board. Are any options that T1024RDB has something similar ?

 

When I boot up the system I see the next :

 

U-Boot 2016.012.0+ga9b437f (Sep 13 2016 - 16:36:48 -0400)

 

CPU0:  T1024E, Version: 1.0, (0x85480010)

Core:  e5500, Version: 2.1, (0x80241021)

Single Source Clock Configuration

Clock Configuration:

       CPU0:1400 MHz, CPU1:1400 MHz,

       CCB:400  MHz,

       DDR:800  MHz (1600 MT/s data rate) (Asynchronous), IFC:100  MHz

       QE:200  MHz

       FMAN1: 700 MHz

       QMAN:  400 MHz

L1:    D-cache 32 KiB enabled

       I-cache 32 KiB enabled

Reset Configuration Word (RCW):

       00000000: 0810000e 00000000 00000000 00000000

       00000010: 4a800003 80000012 ec027000 21000000

       00000020: 00000000 00000000 00000000 00030810

       00000030: 00000000 0b005a08 00000000 00000006

I2C:   ready

Board: T1024RDB, Board rev: 0x03 CPLD ver: 0x07, boot from NOR vBank0

SERDES Reference Clocks:

SD1_CLK1=156.25MHZ, SD1_CLK2=100.00MHZ

SPI:   ready

DRAM:  Initializing....using SPD

Detected UDIMM 18KSF51272AZ-1G6K1

2 GiB left unmapped

4 GiB (DDR3, 64-bit, CL=11, ECC on)

       DDR Chip-Select Interleaving Mode: CS0+CS1

Flash: 128 MiB

L2:    256 KiB enabled

Corenet Platform Cache: 256 KiB enabled

Using SERDES1 Protocol: 149 (0x95)

SEC0: RNG instantiated

NAND:  1024 MiB

MMC:   FSL_SDHC: 0

Firmware 'Microcode version 0.0.1 for T1024 r1.0' for 1024 V1.0

QE: uploading microcode 'Microcode for T1024 r1.0' version 0.0.1

EEPROM: Invalid ID (ff ff ff ff)

PCIe1: Root Complex, no link, regs @ 0xfe240000

PCIe1: Bus 00 - 00

PCIe2: Root Complex, no link, regs @ 0xfe250000

PCIe2: Bus 01 - 01

PCIe3: Root Complex, no link, regs @ 0xfe260000

PCIe3: Bus 02 - 02

In:    serial

Out:   serial

Err:   serial

Net:   Fman1: Uploading microcode version 108.4.5

 

Why I’m getting EEPROM  Invalid ?

I found something  in uboot , but it didn’t work.  

 

 

=> i2c help

i2c - I2C sub-system

 

Usage:

i2c bus [muxtype:muxaddr:muxchannel] - show I2C bus info

crc32 chip address[.0, .1, .2] count - compute CRC32 checksum

i2c dev [dev] - show or set current I2C bus

i2c loop chip address[.0, .1, .2] [# of objects] - looping read of device

i2c md chip address[.0, .1, .2] [# of objects] - read from I2C device

i2c mm chip address[.0, .1, .2] - write to I2C device (auto-incrementing)

i2c mw chip address[.0, .1, .2] value [count] - write to I2C device (fill)

i2c nm chip address[.0, .1, .2] - write to I2C device (constant address)

i2c probe [address] - test for and show device(s) on the I2C bus

i2c read chip address[.0, .1, .2] length memaddress - read to memory

i2c write memaddress chip address[.0, .1, .2] length [-s] - write memory

          to I2C; the -s option selects bulk write in a single transaction

i2c reset - re-init the I2C Controller

i2c speed [speed] - show or set I2C bus speed

 

=> i2c md 0x50 0 0x10

0000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................

 

=> i2c mw 0x50 0x0 0x18 0x10

 

=> i2c md 0x50 0 0x10

0000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................

 

=> i2c mm 0x50 0

00000000: ff ? 11

00000001: ff ? 12

00000002: ff ? 13

00000003: ff ? 14

00000004: ff ? =>

00000004: ff ? q

 

=> i2c md 0x50 0 0x10

0000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................

 

=> md 0xffdf0050

ffdf0050: 00000000 0f000131 02000000 00000000    .......1........

ffdf0060: 55aa0307 00000000 00000000 00000000    U...............

=> mw.b 0xffdf0050 0x8

=> i2c mm 0x50 0x0

00000000: ff ? 01

00000001: ff ? 02

00000002: ff ? 03

00000003: ff ? 04

00000004: ff ? q

=> i2c md 0x50 0 0x10

0000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................

=> i2c mw 0x50 0x0 0x18 0x10

=> i2c md 0x50 0 0x10

0000: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................

=>

 

No matter what I did it return FF all the time .

Any inputs?

Thank you.

0 项奖励
回复
5 回复数

1,734 次查看
bpe
NXP Employee
NXP Employee

The message your u-Boot displays about invalid ID is not an indication
of any serious problem. u-Boot attempts to read a certain structure
from the onboard EEPROM and doesn't find it there. There is no critical
info in that structure. For details, see common/cmd_mac.c and
board/freescale/common/sys_eeprom.c

I'm not sure why you are unable to program your EEPROM, the commands
you are entering seem valid. In case your u-Boot is improperly configured
for the address size, try specifying it explicitly, the EEPROM expects
two-byte addresses, i.e. "mw 0x50 4.2 ...".


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,734 次查看
valentinmovsik
Contributor I

Hi Platon,

Thanks for help.

Please take a look in what I did :

1. => eeprom help
eeprom - EEPROM sub-system

Usage:
eeprom read  <bus> <devaddr> addr off cnt
eeprom write <bus> <devaddr> addr off cnt
       - read/write `cnt' bytes from `devaddr` EEPROM at offset `off'

2. Read from EEProm

=> eeprom read 50  0 0 10

EEPROM @0x50 read: addr 00000000  off 0000  count 16 ... done

3. Read from memory

=> md 0
00000000: ffffffff ffffffff ffffffff ffffffff    ................
00000010: deadbeef deadbeef deadbeef deadbeef    ................
00000020: deadbeef deadbeef deadbeef deadbeef    ................
00000030: deadbeef deadbeef deadbeef deadbeef    ................

I see exactly the same FFFFFF.....

4. Now I'm trying to write into EEPROM from memory 0x10 which is " deadbeef deadbeef deadbeef deadbeef" with offset 0x10 (16 bytes)

=> eeprom write 0x50 0x10 0 10

EEPROM @0x50 write: addr 00000010  off 0000  count 16 ... done

5. And now I'll read back what I've just wrotten :

eeprom read 55 0 0 10

EEPROM @0x55 read: addr 00000000  off 0000  count 16 ... done

6.

=> md 0
00000000: ffffffff ffffffff ffffffff ffffffff    ................

Again FFFFFFFFFFFFFFFF....

0 项奖励
回复

1,734 次查看
bpe
NXP Employee
NXP Employee

Based on the EEPROM chip documentation (www.atmel.com/Images/doc0670.pdf),
it accpets either a single byte write or a page of 64 bytes write.
Both work as expected:

=> i2c md 50 0.2 10
0000: 4e 58 49 44 30 78 37 30 00 00 00 00 00 00 00 00    NXID0x70........
=> i2c mw 50 0.2 1 1
=> i2c md 50 0.2 10
0000: 01 58 49 44 30 78 37 30 00 00 00 00 00 00 00 00    .XID0x70........

=> i2c md 50 0.2 40
0000: 01 58 49 44 30 78 37 30 00 00 00 00 00 00 00 00    .XID0x70........
0010: ff ff ff ff ff ff ff ff ff ff ff ff 00 00 00 01    ................
0020: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................
0030: ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff    ................
=> i2c mw 50 0.2 0a 40
=> i2c md 50 0.2 40
0000: 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a    ................
0010: 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a    ................
0020: 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a    ................
0030: 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a 0a    ................


Arbitrary byte count writes don't work, as you have already found.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,734 次查看
valentinmovsik
Contributor I

Ok ... I got it. I forgot to double check about write operation. As you told it supports only byte or page (64 bytes) write operation.

Now it works fine.

Thanks for help.

Val

0 项奖励
回复

1,734 次查看
valentinmovsik
Contributor I

Some extra information .

The i2c probe return :

=> i2c probe
Valid chip addresses: 00 19 31 40 4D 50 51 68 6A

So , I've tried to read from chip 0x68 which is RTC...

=> i2c md 0x68 0 0x10
0000: 41 11 21 02 21 91 16 00 00 00 00 00 00 00 3c 00    A.!.!.........<.

I2C bus works fine.

0 项奖励
回复