T1024 RDB takes 5 min to start Klogd.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 RDB takes 5 min to start Klogd.

447 Views
kirankumartanka
Contributor I

I am trying to boot T1024RDB based custom board. BSP has bitbaked from SDK1.9. The board is booting ,but Starting of Klogd is taking more than 5 min. This problem is not seen while booting from SDK1.7.What can be the reason?

Following is the log :

generating ssh ED25519 key...
done.
Error: There is no config file for conntrackd
Starting network benchmark server: netserver.
Starting system log daemon...0
Starting kernel log daemon...1
Starting internet superserver: xinetd.

Please help me to fix this problem.

Thanks & Regards,

0 Kudos
1 Reply

346 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Kiran Kumar Tankala ,

Please refer to my following log, I boot T1024RDB with the core image filesystem from SDK 1.9 prebuilt image ISO, and didn't reproduce your problem.

According to your log, there is no config file for conntrackd, how did you built the filesystem image? What did you modified? Did you boot filesystem from RAM or Flash? I am afraid your filesystem image is not entire, probably it is overridden by other image.

INIT: Entering runlevel: 5
Configuring network interfaces... done.
Starting OpenBSD Secure Shell server: sshd
  generating ssh RSA key...
  generating ssh ECDSA key...
  generating ssh DSA key...
  generating ssh ED25519 key...
done.
Starting network benchmark server: netserver.
Starting system log daemon...0
Starting kernel log daemon...0
Starting internet superserver: xinetd.

QorIQ SDK (FSL Reference Distro) 1.9 t1024rdb /dev/ttyS0

t1024rdb login: root

Thanks,

Yiping

0 Kudos