I am working on schematics for a HW design for a new product that is targetting the LS1046A. I need to configure the JTAG interface so I can bring up the prototype designs. I searching for what JTAG pods or interfaces are supported. Searching the web, everything seems to point back to Code Warrior TAP.
Questions:
1. What JTAG interfaces support the LS1046A? I have a J-Link Plus, but Segger said that it does not support LS1046A because they could not get the necessary documentation.
2. Is the only interface to these parts through Code Warrior and Code Warrior TAP?
Thank you.
Solved! Go to Solution.
1) NXP supports only CodeWarrior IDE and CodeWarrior TAP + ARM Probe Tip:
2) Lauterbach Trace32 supports LS1046A:
1) NXP supports only CodeWarrior IDE and CodeWarrior TAP + ARM Probe Tip:
2) Lauterbach Trace32 supports LS1046A: