Serdes1 is configured as USXGMII and PCIE, but uboot cannot be started.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serdes1 is configured as USXGMII and PCIE, but uboot cannot be started.

44 Views
Zhoute
Contributor I

Hi,Dear NXP developers: 尊敬的NXP开发者们: 

Currently, the PLLF clock input is 156.25M, and the PLLS clock input is 100M.Serdes 1 I am using the mode of 16H, USXGMII and PCIE.After enabling PLL0 (PLLF), the serial port stopped printing directly. After disabling PLL0, the printing was normal. Could you please advise on how to handle this issue? The following is my rcw configuration and my log print.目前,PLLF时钟输入为156.25M, PLLS时钟输入为100M。服务器1我使用16H, USXGMII和PCIE模式。使能PLL0 (PLLF)后,串口直接停止打印。禁用PLL0后,打印正常。请问如何处理这个问题?以下是我的rcw配置和日志打印。

LX2160A-RDB 

0 Kudos
Reply
0 Replies