SODIMM with LS1088A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SODIMM with LS1088A

929 次查看
mustafa
Contributor I

Hi There,

I am looking to custom design a board with QorIQ  Processing Platform with LS1088A. I do not have any issue of using the DDR4 but I would rather use SODIMM due to being small in size.

I am doing some preliminary research on the device itself. It looks like I can use x72 ECC SODIMM DDR4.

Can anyone please let me know if there is any serious concern on using SODIMM instead of DIMM.

Is there any crucial signals that are not connected on the SODIMM RAM module might effect the design.

Regards

#ddr4#ddr4 ecc#qoriq ls1088a#ls1088a#dimm#so-dimm

0 项奖励
回复
1 回复

800 次查看
Bulat
NXP Employee
NXP Employee

There are no concerns whether DDR4 DIMM or SODIMM is used. Both x72 DIMM and x72 SODIMM have the same set of signals, so the design would be identical.

Regards,

Bulat

0 项奖励
回复