SEC hardware is failing at high throughput (over 30 Mbps)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SEC hardware is failing at high throughput (over 30 Mbps)

458 Views
samirsamaha
Contributor II

Hi,

I am using the SEC driver (TALITOS P1020) to encrypt and decrypt the data. I am using SDK1.9 and the AEAD interface crypto_aead_encrypt() and crypto_aead_decrypt() functions. The decryption completion is failing at high throughput (over 30 Mbps). From time to time the function ipsec_esp_decrypt_hwauth_done() returns EBADMSG. In this function the desc->hdr_lo is equal to DESC_HDR_LO_ICCR1_FAIL. It looks like the hardware is failing. Is there any idea what could make the hardware to return this kind of error?

Regards,

Samir Samaha

0 Kudos
1 Reply

301 Views
bpe
NXP Employee
NXP Employee

Discussing this issue requires references to NDA documentation, which is  not possible here.

Please create a Support Case for it:

https://community.nxp.com/docs/DOC-329745 


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos