SDK and BSP questions for LS2160ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK and BSP questions for LS2160ARDB

1,255 次查看
linj17
Contributor I

I have a ls2160ardb. This is from the boot log "QorIQ SDK (FSL Reference Distro) 2.5 lx2160ardb /dev/ttyAMA0". 

Questions:

1, What is the version of BSP?

2, What SDK should I use for this BSP?

3, If I want to upgrade to latest BSP 0.5, where can I get the latest BSP and  LX2160ARDB composite firmware image?

Thanks,

Nancy.

0 项奖励
回复
1 回复

1,093 次查看
ufedor
NXP Employee
NXP Employee

Current public NXP LSDK v19.03 supports the LX2160A.
All previous BSPs are obsolete.

The LSDK is available at:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...
Composite firmware images are available at:

https://lsdk.github.io/components.html

tab "LSDK IMAGES".

The firmware image to boot lx2160ardb board from SD card with u-boot:

firmware_lx2160ardb_uboot_sdboot.img

The firmware image to boot lx2160ardb board from XSPI flash with u-boot:

firmware_lx2160ardb_uboot_xspiboot.img

0 项奖励
回复