I want to run usdpaa reflector on ls1043a-rdb. I flashed SDK 2.0 prebuilt image kernel_usdpaa.itb and ls1043ardb/RR_FQPP_1455/rcw_1600.bin to bank4. I did not flash Image--4.1-r0-fsl-ls1043a-rdb-usdpaa-20160515025831.dtb because I believe the .itb file has it included. It boots up to linux. Questions:
1 - from linux ifconfig -a lists no interfaces, therefore I assume all 7 interfaces (6 x 1Gbps + 1 x 10Gbps) belong to usdpaa partition? How can I view belong to usdpaa partition interfaces and assign ip addresses to them?
2 - starting reflector gives below error. full boot log is attached. What am I doing wrong?
root@ls1043ardb:~# cat /root/SOURCE_THIS
cd /usr/etc
fmc -c usdpaa_config_p4_serdes_0xe.xml -p usdpaa_policy_hash_ipv4.xml -a
reflector
root@ls1043ardb:~# source /root/SOURCE_THIS
ERR : Invocation of FM_Open for fm1 failed
ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010028
Found /fsl,dpaa/dpa-fman0-oh@2, Tx Channel = 80a, FMAN = 0, Port ID = 1
Found /fsl,dpaa/ethernet@0, Tx Channel = 802, FMAN = 0, Port ID = 1
Found /fsl,dpaa/ethernet@1, Tx Channel = 803, FMAN = 0, Port ID = 2
Found /fsl,dpaa/ethernet@2, Tx Channel = 804, FMAN = 0, Port ID = 3
Found /fsl,dpaa/ethernet@3, Tx Channel = 805, FMAN = 0, Port ID = 4
Found /fsl,dpaa/ethernet@4, Tx Channel = 806, FMAN = 0, Port ID = 5
Found /fsl,dpaa/ethernet@5, Tx Channel = 807, FMAN = 0, Port ID = 6
Found /fsl,dpaa/ethernet@8, Tx Channel = 800, FMAN = 0, Port ID = 9
QMan: Allocated lookup table at 0xffff902e1010, entry count 32769
Configuring for 1 network interface
Allocated DMA region size 0x1000000
reflector starting
Released 0 bufs to BPID 7
Released 0 bufs to BPID 8
cpu hotplug daemon not running: No such file or directory
Released 4096 bufs to BPID 9
Data stashing: Enabled
Thread uid:0 alive (on cpu 1)
3 - Is there a performance difference between PPAC-based hello_reflector and hello_reflector?
Thank you,
Bob
Original Attachment has been moved to: ls1043-rdb-usdpaa-boot-log.txt.zip