SATA support for TWR-LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SATA support for TWR-LS1021A

2,009 Views
jianwu
Contributor II

Hello,

I used SD card boot TWR_LS1021 board. I connect TWR-LS1021A with external hard driver. But u-boot cannot detect it. The below is my u-boot log:

U-Boot 2015.01+ls1+g6ba8eed (Sep 01 2015 - 13:21:32)

CPU:   Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 20000000 00407900 60040a00 21046000

       00000020: 00000000 00000000 00000000 00038000

       00000030: 00080000 881b7340 00000000 00000000

Board: LS1021ATWR

CPLD:  V2.2

PCBA:  V3.0

VBank: 0

I2C:   ready

DRAM:  1 GiB

Using SERDES1 Protocol: 32 (0x20)

Flash: 128 MiB

MMC:   FSL_SDHC: 0

PCIe1: Root Complex no link, regs @ 0x3400000

PCIe2: Root Complex no link, regs @ 0x3500000

In:    serial

Out:   serial

Err:   serial

SEC0: RNG instantiated

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

Found 0 device(s).

SCSI:  Net:   eTSEC1 is in sgmii mode.

eTSEC2 is in sgmii mode.

eTSEC1, eTSEC2, eTSEC3 [PRIME]

=>

What is the correct RCW for SD boot and support SATA, USB etc?

Can anybody send me an u-boot image for sd boot and support SATA3.0 device detect?

Thanks,

Jian

10 Replies

1,824 Views
jianwu
Contributor II

I got SATA works on my LS1021TWR.

Thank Sinan and Yiping's help,

Regards,

Jian

0 Kudos
Reply

1,824 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Jian Wu,

You didn't enable SATA in RCW, please refer to the following SerDes options for RCW[128:135].

pastedImage_1.png

Please use RSR_PPS_70 RCW provided in the prebuilt images ISO.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,824 Views
jianwu
Contributor II

Hi Yiping,

Thanks for your help.

Once I boot up LS1021twr with SD card, how can I update RCW with your attached rcw_1000.bin?

Thanks,

Jian

0 Kudos
Reply

1,824 Views
jianwu
Contributor II

Any answer and help?

Thanks,

Jian

0 Kudos
Reply

1,824 Views
jianwu
Contributor II

Any help will be appreciated.

Thanks,

Jian

0 Kudos
Reply

1,824 Views
sinanakman
Senior Contributor III

Hi Jian

Can you try this with mainline u-boot and see

if it works. If you have problem with mainline

u-boot, you could then also ask in u-boot mailing

list and I can be also more help as I am more familiar

with mainline u-boot.

Please give it a try with mainline u-boot.

Regards

Sinan Akman

0 Kudos
Reply

1,824 Views
jianwu
Contributor II

Hi Sinan,

Thanks for your help.

Can you attach your mainline u-boot image binary for sd boot for me?

Many thanks,

Jian

0 Kudos
Reply

1,824 Views
sinanakman
Senior Contributor III

Hi Jian

I don't think there is a way for me to attach a binary file here.

You can generate the binary image yourself :

git clone git://git.denx.de/u-boot.git u-boot/

cd u-boot

git checkout v2015.10

make distclean

make ls1021atwr_sdcard_defconfig

make all

the binary file you need is : u-boot-with-spl-pbl.bin

Try building the image and this way you can also

debug it if it is failing.

If you have problems, send your e-mail address and

I will e-mail you the binary file.

Regards

Sinan Akman

0 Kudos
Reply

1,823 Views
jianwu
Contributor II

Hi Sinan,

Thanks  a lot for your help.

I got problem to build the SD: u-boot.bin. Could you please send me your SD u-boot binary to try?

My email: jianwu@qnx.com

Thanks a lot,

Jian

0 Kudos
Reply

1,823 Views
sinanakman
Senior Contributor III

Hi Jian

What kind of problems did you have building the u-boot binary.

Can you please send me your build errors.

I will send you the binary in a separate e-mail.

Did Yiping's suggestion not help ?

Please show your build errors here that we can help.

Regards

Sinan Akman

0 Kudos
Reply