Reset the DPAA on the P2041 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reset the DPAA on the P2041 processor

1,375 次查看
benjaminbar-kov
Contributor I

The support from our RTOS provider claimed that -

"queue manager and frame manager cannot be reset  and so the dpaa network cannot be reset."

is it so ??? And if it is not so, what is the best way to reset the dpaa after using it some time, and then reset it and start using it again, without reseting the application.

0 项奖励
回复
2 回复数

1,107 次查看
Goker
Contributor I

The question is so old but did you find a way to restart DPAA? 

0 项奖励
回复

1,233 次查看
LPP
NXP Employee
NXP Employee

In fact, it is possible to perform "warm" reset of DPAA but it is not documented in DPAARM and P2041RM. The warm reset may not completely reinitialize the logic the way a Hard Reset will.

I'm not sure if this functionality is widely demanded. If you want to obtain more information on this functionality, please, create a service request to NXP support.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------