Re: T2080 processor DDR3 initilalization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: T2080 processor DDR3 initilalization

440 Views
vidyasagartata
Contributor II

Dear flaby & pavel,

 

I have same issue in our custom T2080 design in discrete DDR3 chip configuration.

 

I have modified t2080rdb configuration file and board/freescale/t208xrdb/ddr.c for DDR3 discrete chip configuration.

 

But uboot gets hang after returning the ddr data rate.

 

"DRAM:  Initializing....Configuring DDR for 1066.640 MT/s data rate"

 

We have verified ddr timing parameter from QCVS tool, able to get read and write within memory range 0x00000000 - 0x7fffffff.

 

Please find the modified configuration file in attachment and below is the u-boot log.

 

I am using SDK2.0 for development.

 

If i enable "dram_size = fsl_ddr_sdram_size();" in the ddr.c file getting only "ddr size = 1000000" size.

 

 

U-Boot 2016.01 (May 26 2017 - 08:52:23 +0530)

 

CPU0:  T2080E, Version: 1.1, (0x85380011)
Core:  e6500, Version: 2.0, (0x80400120)
Clock Configuration:
       CPU0:533.333 MHz, CPU1:533.333 MHz, CPU2:533.333 MHz, CPU3:533.333 MHz,
       CCB:533.333 MHz,
       DDR:533.320 MHz (1066.640 MT/s data rate) (Asynchronous), IFC:133.333 MHz
       FMAN1: 266.667 MHz
       QMAN:  266.667 MHz
       PME:   533.333 MHz
L1:    D-cache 32 KiB enabled
       I-cache 32 KiB enabled
Reset Configuration Word (RCW):
       00000000: 10040008 08000000 00000000 00000000
       00000010: 6c290002 70004200 fc027000 41000000
       00000020: 00800000 00000000 00000000 000323fc
       00000030: 00000100 00800009 00000000 00000004
I2C:   ready
Board: T2080RDB, Board rev: 0xff CPLD ver: 0xff, boot from NOR vBank1
SERDES Reference Clocks:
SD1_CLK1=156.25MHZ, SD1_CLK2=125.00MHz
SD2_CLK1=125.00MHz, SD2_CLK2=125.00MHz
SPI:   ready
DRAM:  Initializing....Configuring DDR for 1066.640 MT/s data rate

 

Please provide your suggestion to make DDR3 discrete chip working.

 

Thanks,

Vidya

Original Attachment has been moved to: T208xRDB.h.zip

Original Attachment has been moved to: ddr.c.zip

0 Kudos
0 Replies