RT8211DN chip support on NXP LS1012A FRDM Board BSP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT8211DN chip support on NXP LS1012A FRDM Board BSP

522 次查看
alpeshmandani
Contributor IV

Hello,

I am working on custom product development using NXP LS1012A and have cosider Realtek RT8211DN ethernet transreciver chip for RGMII and SGMII ethernet interface.

Does NXP LS1012A FRDM Board BSP having support for RT8211DN chip ? Because of Realtek RT8211FS ethernet PHY chips used on NXP LS1012A FRAM board and Realtek doesnt provide support on lower volume as well as proto level.

Thanks,

Regards,

Alpesh Mandai

0 项奖励
1 回复

377 次查看
Pavel
NXP Employee
NXP Employee

NXP SDK 2.0-1703 supports FRDM-LS1012A board. See the Chapter 4.4.6 of NXP SDK 2.0-1703 documentation:

http://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

This SDK supports Ethernet connection using Realtek RT8211DN Ethernet PHY under u-boot and under Linux.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励