RS485 interfacing T2081 Processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RS485 interfacing T2081 Processor

1,855件の閲覧回数
hemanttiwari199
Contributor III

Hello Everyone,

Can any tell me how to interface RS485 Transceiver with T2081 Processor? Any reference design will be really helpful.

Thanks in advance

Regards

Hemant

ラベル(1)
タグ(3)
0 件の賞賛
返信
5 返答(返信)

1,790件の閲覧回数
hemanttiwari199
Contributor III

Hi,

Actually i want to know how i can interface RS485 with T2081? As there is no specific pin for RS485 interface. how can i interface irs485 with UART pin of T2081?

Regards

Hemant

0 件の賞賛
返信

1,790件の閲覧回数
hemanttiwari199
Contributor III

Sorry Typing Error. It is RS485!!

0 件の賞賛
返信

1,790件の閲覧回数
ufedor
NXP Employee
NXP Employee

You have to select an RS485 transceiver IC which can be connected to the T2081 UART signals considering that DVDD could be either 2.5V or 1.8V (refer to the QorIQ T2081 Data Sheet).

0 件の賞賛
返信

1,790件の閲覧回数
ufedor
NXP Employee
NXP Employee

> how can i interface irs485 with UART pin of T2081?

What is the "irs485"?

0 件の賞賛
返信

1,790件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no RS485 reference design for the T2081.

For possible approach please refer to the Community thread:

https://community.nxp.com/message/1002564 

0 件の賞賛
返信