RS485 interfacing T2081 Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RS485 interfacing T2081 Processor

2,645 Views
hemanttiwari199
Contributor III

Hello Everyone,

Can any tell me how to interface RS485 Transceiver with T2081 Processor? Any reference design will be really helpful.

Thanks in advance

Regards

Hemant

Labels (1)
Tags (3)
0 Kudos
Reply
5 Replies

2,580 Views
hemanttiwari199
Contributor III

Hi,

Actually i want to know how i can interface RS485 with T2081? As there is no specific pin for RS485 interface. how can i interface irs485 with UART pin of T2081?

Regards

Hemant

0 Kudos
Reply

2,580 Views
hemanttiwari199
Contributor III

Sorry Typing Error. It is RS485!!

0 Kudos
Reply

2,580 Views
ufedor
NXP Employee
NXP Employee

You have to select an RS485 transceiver IC which can be connected to the T2081 UART signals considering that DVDD could be either 2.5V or 1.8V (refer to the QorIQ T2081 Data Sheet).

0 Kudos
Reply

2,580 Views
ufedor
NXP Employee
NXP Employee

> how can i interface irs485 with UART pin of T2081?

What is the "irs485"?

0 Kudos
Reply

2,580 Views
ufedor
NXP Employee
NXP Employee

There is no RS485 reference design for the T2081.

For possible approach please refer to the Community thread:

https://community.nxp.com/message/1002564 

0 Kudos
Reply