QorlQ T2080 Eval Board IFC and CPLD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorlQ T2080 Eval Board IFC and CPLD

845 Views
KLN
Contributor III

Hi,

What is the purpose of connecting IFC to CPLD in QorlQ T2080 Evaluation board?

KLN_0-1677038885773.pngKLN_1-1677038900465.pngKLN_2-1677038920751.png

 

0 Kudos
Reply
3 Replies

818 Views
yipingwang
NXP TechSupport
NXP TechSupport

• CPLD
— PCBA version identify
— Manages system power and reset sequencing
— Configures DUT, board, clock with dynamic
— Reset and interrupt monitor and control
— General fault monitoring and logging

The IFC GPCM interface is used to access the registers of CPLD and FPGA.

0 Kudos
Reply

815 Views
KLN
Contributor III

I'm still unclear on what kind of use case especially IFC interface between CPLD and NXP T2080.

 

0 Kudos
Reply

750 Views
yipingwang
NXP TechSupport
NXP TechSupport

There are many reasons:

1) Many POR config pins (cfg_*_*) are multiplexed with IFC pins. FPGA ensures these pins are in desired state during POR

2) Single NOR flash has been divided in two banks. Implies user can have boot code in Bank 0 and Bank 4. This is done by FPGA by inverting the MSB of address line

3) If user wants to boot from NAND or NOR, FPGA can re-route CS0 accordingly

4) Converntionally, registers implemented in FPGA could be accessed through FPGA

5) Some of the modes of IFC which cannot be tested using existing flashes, can be implemented on FPGA during validation phase...

0 Kudos
Reply