QorIQ SDK 1.8, Compiling MacSec as a module, T1024RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ SDK 1.8, Compiling MacSec as a module, T1024RDB

1,943件の閲覧回数
florianbraun
Contributor I

Hello, I am trying to compile MacSec as a module as shown in the QorIQ SDK Documentation:

Device Drivers

+-> Network device support (NETDEVICES [=y])

+-> Ethernet driver support (ETHERNET [=y])

+-> Freescale devices (NET_VENDOR_FREESCALE [=y])

+-> DPAA Ethernet (FSL_DPAA_ETH [=y])

+-> DPAA Macsec [=m]

but +-> Freescale devices (NET_VENDOR_FREESCALE [=y]) does not show up for me.

i used "make menuconfig" in ".../poky/build_t1024../tmp/sysroots/t1024rdb/usr/src/kernel

So how do i go about activating MacSec on my t1024rdb?

edit: figured it out, thank you

0 件の賞賛
返信
1 返信

1,804件の閲覧回数
Pavel
NXP Employee
NXP Employee

There is no similar problem if SDK 1.9 is used. Use this SDK.

See attached files.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信