Hi,
I have two questions about QorIQ B4860 processor.
1) I want to run Ubuntu/ Windows on QorIQ B4860 processor. So is there any GPU available in this processor so that I can boot GUI based OS and can run some multimedia application on this processor.
2) I was looking for a board with QorIQ B4860 processor and I found QorIQ B4860BDS board with this processor. But I can't find any schematic and Board layout for this board. Is there any schematic and board layout available for this board? If yes how can I get those files?
Solved! Go to Solution.
1) B4860 does not possess GPU.
2) Schematics is confidential and can be provided only under NDA.
NDA signing can be arranged by creating a Technical Case using corporate email:
Thanks for your reply.
1) B4860 does not possess GPU.
2) Schematics is confidential and can be provided only under NDA.
NDA signing can be arranged by creating a Technical Case using corporate email:
There is no new design for the B4860 - please refer to the information provided by the following link: