QoIQ T4240RDB-64bit boot error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QoIQ T4240RDB-64bit boot error

1,349 Views
hosytan
Contributor III

Hello,

I am booting my QoIQ T4240RDB using Freescale SDK 2.0 but kernel hangs with the following error.

This is my shell to start QEMU in Linux Ubuntu 14.04 LTS:

sudo ~/nxp/run/QorIQ-SDK-V2.0-20160527-yocto/build_t4240rdb-64b/tmp/sysroots/x86_64-linux/usr/bin/qemu-system-ppc64 \
-cpu e5500 -nographic -m 1024 -M ppce500 \
-kernel ~/nxp/run/QorIQ-SDK-V2.0-20160527-yocto/build_t4240rdb-64b/tmp/deploy/images/t4240rdb-64b/uImage \
--initrd ~/nxp/run/QorIQ-SDK-V2.0-20160527-yocto/build_t4240rdb-64b/tmp/deploy/images/t4240rdb-64b/fsl-image-core-t4240rdb-64b.ext2.gz \
--append "root=/dev/ram rw console=ttyS0,115200 \
ip=26.26.26.2::26.26.26.1:255.255.255.0 mem=1024M ramdisk_size=500000" -serial tcp::4444,server,telnet -net nic,model=e1000 \
-net tap,ifname=tap0,script=no,downscript=no

When telnet to QEMU Guest, this is booting logs:

~$ telnet 26.26.26.1 4444
Trying 26.26.26.1...
Connected to 26.26.26.1.
Escape character is '^]'.
Using QEMU e500 machine description
MMU: Supported page sizes
4 KB as direct
4096 KB as direct
16384 KB as direct
65536 KB as direct
262144 KB as direct
1048576 KB as direct
MMU: Book3E HW tablewalk not supported
Found initrd at 0xc000000004000000:0xc000000004424a00
bootconsole [udbg0] enabled
CPU maps initialized for 1 thread per core
Starting Linux PPC64 #1 SMP Wed Jan 25 13:07:02 ICT 2017
-----------------------------------------------------
ppc64_pft_size = 0x0
phys_mem_size = 0x40000000
dcache_line_size = 0x40
icache_line_size = 0x40
cpu_features = 0x00180400181802c0
possible = 0x00180480581802c8
always = 0x00180400581802c0
cpu_user_features = 0xcc008000 0x08000000
mmu_features = 0x000a0010
firmware_features = 0x0000000000000000
-----------------------------------------------------
<- setup_system()
Linux version 4.1.30-rt34+g4004071 (hstan@hstan-ubuntu) (gcc version 4.9.2 (GCC) ) #1 SMP Wed Jan 25 13:07:02 ICT 2017
qemu_e500_setup_arch()
Zone ranges:
DMA [mem 0x0000000000000000-0x000000003fffffff]
DMA32 empty
Normal empty
Movable zone start for each node
Early memory node ranges
node 0: [mem 0x0000000000000000-0x000000003fffffff]
Initmem setup node 0 [mem 0x0000000000000000-0x000000003fffffff]
MMU: Allocated 2112 bytes of context maps for 255 contexts
PERCPU: Embedded 17 pages/cpu @c00000003f000000 s28824 r0 d40808 u1048576
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 258560
Kernel command line: root=/dev/ram rw console=ttyS0,115200 ip=26.26.26.2::26.26.26.1:255.255.255.0 mem=1024M ramdisk_size=500000
PID hash table entries: 4096 (order: 3, 32768 bytes)
Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
Sorting __ex_table...
Memory: 949000K/1048576K available (7872K kernel code, 1144K rwdata, 3016K rodata, 360K init, 764K bss, 99576K reserved, 0K cma-reserved)
Hierarchical RCU implementation.
RCU debugfs-based tracing is enabled.
CONFIG_RCU_FANOUT set to non-default value of 32
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=24 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at fe0040000, max 1 CPUs
mpic: ISU size: 256, shift: 8, mask: ff
mpic: Initializing for 256 sources
clocksource timebase: mask: 0xffffffffffffffff max_cycles: 0x5c4093a7d1, max_idle_ns: 440795210635 ns
clocksource: timebase mult[2800000] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 2048 (order: 2, 16384 bytes)
Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes)
e500 family performance monitor hardware support registered
Brought up 1 CPUs
devtmpfs: initialized
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
xor: measuring software checksum speed
8regs : 1679.000 MB/sec
8regs_prefetch: 1413.000 MB/sec
32regs : 1699.000 MB/sec
32regs_prefetch: 1348.000 MB/sec
xor: using function: 32regs (1699.000 MB/sec)
NET: Registered protocol family 16
Found FSL PCI host bridge at 0x0000000fe0008000. Firmware bus number: 0->255
PCI host bridge /pci@fe0008000 (primary) ranges:
MEM 0x0000000c00000000..0x0000000c1fffffff -> 0x00000000e0000000
IO 0x0000000fe1000000..0x0000000fe100ffff -> 0x0000000000000000
/pci@fe0008000: PCICSRBAR @ 0xdff00000
setup_pci_atmu: end of DRAM 40000000
EDAC PCI0: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV fe0008000.pci (INTERRUPT)
MPC85xx_edac acquired irq 24 for PCI Err
MPC85xx_edac PCI err registered
fsl-pamu: fsl_pamu_init: could not find a PAMU node
PCI: Probing PCI hardware
fsl-pci fe0008000.pci: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
pci_bus 0000:00: root bus resource [mem 0xc00000000-0xc1fffffff] (bus address [0xe0000000-0xffffffff])
pci_bus 0000:00: root bus resource [bus 00-ff]
pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
pci 0000:00:00.0: PCI bridge to [bus 01-ff]
PCI: Cannot allocate resource region 0 of device 0000:00:00.0, will remap
pci 0000:00:00.0: BAR 0: assigned [mem 0xc00000000-0xc000fffff]
pci 0000:00:00.0: BAR 8: assigned [mem 0xc00100000-0xc001fffff]
pci 0000:00:01.0: BAR 6: assigned [mem 0xc00200000-0xc0023ffff pref]
pci 0000:00:01.0: BAR 0: assigned [mem 0xc00240000-0xc0025ffff]
pci 0000:00:01.0: BAR 1: assigned [io 0x11000-0x1103f]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0: bridge window [io 0x10000-0x10fff]
pci 0000:00:00.0: bridge window [mem 0xc00100000-0xc001fffff]
raid6: int64x1 gen() 641 MB/s
raid6: int64x1 xor() 384 MB/s
raid6: int64x2 gen() 799 MB/s
raid6: int64x2 xor() 604 MB/s
raid6: int64x4 gen() 1106 MB/s
raid6: int64x4 xor() 784 MB/s
raid6: int64x8 gen() 556 MB/s
raid6: int64x8 xor() 382 MB/s
raid6: using algorithm int64x4 gen() 1106 MB/s
raid6: .... xor() 784 MB/s, rmw enabled
raid6: using intx1 recovery algorithm
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
EDAC MC: Ver: 3.0.0
No BMan portals available!
QMan: Allocated lookup table at 8000000000002000, entry count 65537
No QMan portals available!
No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
Switched to clocksource timebase
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 5, 131072 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 4240K (c000000004000000 - c000000004424000)
futex hash table entries: 256 (order: 2, 16384 bytes)
audit: initializing netlink subsys (disabled)
audit: type=2000 audit(1.184:1): initialized
HugeTLB registered 4 MB page size, pre-allocated 0 pages
HugeTLB registered 16 MB page size, pre-allocated 0 pages
HugeTLB registered 64 MB page size, pre-allocated 0 pages
HugeTLB registered 256 MB page size, pre-allocated 0 pages
HugeTLB registered 1 GB page size, pre-allocated 0 pages
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
ntfs: driver 2.1.32 [Flags: R/O].
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
async_tx: api initialized (async)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
console [ttyS0] disabled
serial8250.0: ttyS0 at MMIO 0xfe0004500 (irq = 42, base_baud = 115200) is a 16550A
console [ttyS0] enabled
console [ttyS0] enabled
bootconsole [udbg0] disabled
bootconsole [udbg0] disabled
ePAPR hypervisor byte channel driver
brd: module loaded
loop: module loaded
st: Version 20101219, fixed bufsize 32768, s/g segs 256
libphy: Fixed MDIO Bus: probed
Freescale FM module, FMD API version 21.1.0
Freescale FM Ports module
fsl_mac: fsl_mac: FSL FMan MAC API based driver
fsl_dpa: FSL DPAA Ethernet driver
fsl_advanced: FSL DPAA Advanced drivers:
fsl_proxy: FSL DPAA Proxy initialization driver
fsl_dpa_shared: FSL DPAA Shared Ethernet driver
fsl_dpa_macless: FSL DPAA MACless Ethernet driver
fsl_oh: FSL FMan Offline Parsing port driver
e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
e1000e: Copyright(c) 1999 - 2014 Intel Corporation.
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
usbcore: registered new interface driver usb-storage
i2c /dev entries driver
md: raid6 personality registered for level 6
md: raid5 personality registered for level 5
md: raid4 personality registered for level 4
Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
No fsl,qman node
Freescale USDPAA process driver
fsl-usdpaa: no region found
Freescale USDPAA process IRQ driver
dce_sys_init done!
No fsl,dce node
Freescale pme2 db driver
PME2: fsl_pme2_db_init: not on ctrl-plane
Freescale pme2 scan driver
fsl-pme2-scan: device pme_scan registered
Freescale hypervisor management driver
fsl-hv: no hypervisor found
ipip: IPv4 over IPv4 tunneling driver
Initializing XFRM netlink socket
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
fsl_generic: FSL DPAA Generic Ethernet driver
hctosys: unable to open rtc device (rtc0)
md: Skipping autodetection of RAID arrays. (raid=autodetect will force)
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing unused kernel memory: 360K (c000000000aa9000 - c000000000b03000)
init[1]: unhandled signal 4 at 00003fff947ef0fc nip 00003fff947ef0fc lr 00003fff947d0d94 code 30001
Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004

CPU: 0 PID: 1 Comm: init Not tainted 4.1.30-rt34+g4004071 #1
Call Trace:
[c0000000390538c0] [c0000000007a77d8] .dump_stack+0xac/0xec (unreliable)
[c000000039053950] [c0000000007a50d4] .panic+0xf0/0x280
[c0000000390539f0] [c00000000003b608] .do_exit+0xa0c/0xa10
[c000000039053ae0] [c00000000003c6a8] .do_group_exit+0x54/0xec
[c000000039053b70] [c000000000048788] .get_signal+0x2f8/0x674
[c000000039053c70] [c0000000000092bc] .do_signal+0x44/0x218
[c000000039053db0] [c00000000000959c] .do_notify_resume+0x64/0x78
[c000000039053e30] [c000000000000c4c] .ret_from_except_lite+0x78/0x7c
Rebooting in 180 seconds..

 

I have tried to recompile in QorIQ-SDK-2.0 and boot from SD Card on my T4240RDB board but I always get the same error message.

Shall I use a different rootfs or change something in QEMU command or somewhere?

 

Thanks in advance,

 

Regards,

Ho Sy Tan.

2 Replies

643 Views
Pavel
NXP Employee
NXP Employee

SDK 2.0 documentation contains recommendation for KVM/QEMU building:

http://www.nxp.com/assets/documents/data/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

Do you use these recommendations for QEMU building?


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

643 Views
hosytan
Contributor III

Thanks for your reply, Pavel Chubakov.

Do you have any idea when I deployed the results (uImage, rootfs) to T4240rdb-64b board and it have the same errors.

When I booted from sd card on T4240rdb-64b board, I got the same issue:

init[1]: unhandled signal 4 at 00003fff947ef0fc nip 00003fff947ef0fc lr 00003fff947d0d94 code 30001
Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000004

CPU: 0 PID: 1 Comm: init Not tainted 4.1.30-rt34+g4004071 #1
Call Trace:
[c0000000390538c0] [c0000000007a77d8] .dump_stack+0xac/0xec (unreliable)
[c000000039053950] [c0000000007a50d4] .panic+0xf0/0x280
[c0000000390539f0] [c00000000003b608] .do_exit+0xa0c/0xa10
[c000000039053ae0] [c00000000003c6a8] .do_group_exit+0x54/0xec
[c000000039053b70] [c000000000048788] .get_signal+0x2f8/0x674
[c000000039053c70] [c0000000000092bc] .do_signal+0x44/0x218
[c000000039053db0] [c00000000000959c] .do_notify_resume+0x64/0x78
[c000000039053e30] [c000000000000c4c] .ret_from_except_lite+0x78/0x7c
Rebooting in 180 seconds..

Does it relate to qemu or something went wrong?

Please help me resolving my problem.

Thanks in advanced.

0 Kudos
Reply