QCVS Read SPD With multiple devices in JTAG chain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCVS Read SPD With multiple devices in JTAG chain

892 Views
perfranck
Contributor III


Going through the QCVS manual​ to tweak the settings on the DDR4 we have on our LS1020A hardware, and trying to follow the "1.2.3.1 Using Read from SPD option" section. I assume this "Read SPD" assumes the LS1020A is the only thing on the JTAG chain, like with the "Target Connections" under validation?

Which script can I edit to add any generic devices and their bypass info on the JTAG chain?

thanks

0 Kudos
Reply
3 Replies

759 Views
addiyi
NXP Employee
NXP Employee

You already know the scripts (connect.py and connect_call.py).

Adrian

0 Kudos
Reply

759 Views
perfranck
Contributor III

Ah, they use the same scripts? Interesting, because I cannot get it to work. I will have to dig deeper on our end then.

0 Kudos
Reply

759 Views
Pavel
NXP Employee
NXP Employee

Look at attached file. It is JTAG Chapter of the "CW_ARMv7_Targeting_Manual.pdf" file. This file is available in CodeWarrior folder.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply