Please advise about EEE(Energy Efficient Ethernet) on LS1023A(/43A).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please advise about EEE(Energy Efficient Ethernet) on LS1023A(/43A).

1,507件の閲覧回数
kazuyayamauchi
Contributor II

Hi Experts,

We want to support IEEE802.3az (EEE: Energy Efficient Ethernet) on LS1023A(/43A).
From "6.2 mEMAC Features Summary" of LS1043ADPAARM(Rev.0), we understand that the LS1023A can support this.
However, we don't understand how to implement this feature with LS1023A.
Please advise which documents we should reference to.

Also, if any sample code, could you let us know?

Best Regards,

0 件の賞賛
3 返答(返信)

1,249件の閲覧回数
norihiromichiga
Senior Contributor I

Hello, 

ethtools with your suggested option allows us to enable eee, LPI.

>  ethtool --set-eee devname [eee on|off] [tx-lpi on|off] [tx-timer N] [advertise N]

LPI must be supported by hardware block in MAC layer on LS1043A.

Otherwise, above option is meaning less.

Can we think that above option can enable eee (sending LPI, detecting LPI) on MAC layer of LS1043A? 

Of course, we must use Ether PHY with 802.3az along with LS1043A.

Thanks,

Norihiro Michigami

AVNET 

0 件の賞賛

1,249件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no support for LPI on the LS1043.

0 件の賞賛

1,249件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the LSDK Documentation:

ethtool options 

0 件の賞賛