PCIe support in Uboot LX2160A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe support in Uboot LX2160A

2,131 Views
deepanrajanbara
Contributor IV

Hi,

Please let us know, PCIe is driver is supported in uboot. Also how to test the PCIe device is initialized without any issue in uboot.

Does the existing u-boot binary supports PCIe. or is there any sample board configuration in which PCI is enabled and initialized.

Thank you,

Deepanraj.A

Labels (1)
0 Kudos
8 Replies

1,910 Views
ufedor
NXP Employee
NXP Employee

PCIe driver is supported in U-Boot.

You wrote:

> how to test the PCIe device is initialized without any issue in uboot.

U-Boot log will contain a line corresponding to each enabled PCIe controller.

This line will indicate the link training status. Trained link corresponds to properly enumerated EP device.

> Does the existing u-boot binary supports PCIe.

Yes, the LX2160A firmware contains U-Boot supporting PCIe.

0 Kudos

1,910 Views
deepanrajanbara
Contributor IV

PCIe Gen2 and PCIe Gen3 is supported in u-boot ?

0 Kudos

1,910 Views
ufedor
NXP Employee
NXP Employee

Specific PCIe protocol support details are determined by the RCW being used - not U-Boot itself.

0 Kudos

1,910 Views
deepanrajanbara
Contributor IV

Does PCIe support QDMA in linux?

0 Kudos

1,910 Views
ufedor
NXP Employee
NXP Employee

A PCIe controller can be used as source and/or destination of the qDMA - refer to the QorIQ LX2160A Reference Manual, Chapter 24 qDMA.

0 Kudos

1,910 Views
deepanrajanbara
Contributor IV

Hi

Please share me the link to QorIQ LX2160A Reference Manual.

0 Kudos

1,910 Views
ufedor
NXP Employee
NXP Employee

The RM is confidential and can be provided if NDA between NXP and your company is present.

Convenient way is to create a Technical Case:

https://support.nxp.com/s/ 

0 Kudos

1,910 Views
deepanrajanbara
Contributor IV

Please reply for my Question

0 Kudos