P5040: Maximum NAND Flash memory supported

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5040: Maximum NAND Flash memory supported

682 Views
ramchet
Contributor I

Hi,

What is the maximum NAND Flash memory size supported by P5040 QORIQ processor?

0 Kudos
3 Replies

452 Views
Pavel
NXP Employee
NXP Employee

In other words, the P5040 FCM controller supports 2048Bytes page, supports 4 bytes for page addresses and 8 chip-selects.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

452 Views
Pavel
NXP Employee
NXP Employee

The P5040 can use maximum 6 bytes as addresses (eLBC_FMR[AL]) and 8 chip-selects (LCS[n]_B) for NAND Flash. It is limit for NAND Flash size of the P5040.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

452 Views
ufedor
NXP Employee
NXP Employee

The eLBC FCM block address is 3-byte long, so, for 128kB block, maximum supported NAND Flash size for one bank (chip-select) is: 16 M * 128 kB = 2048 GB

0 Kudos