P5020NSE7MMB Processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P5020NSE7MMB Processor?

1,047件の閲覧回数
chockkalingamm
Contributor I

we are using this Processor P5020NSE7MMB one of the our defense project, let me know the processor it will support 1)ARNIC 429 interface (2No)

              2)CAN interface (2No)

              3)RS422 interface(2No)

kindly tell us any alternate solutions.

Thanks & Regards,

Chockkalingam M

0 件の賞賛
返信
1 返信

987件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

1)ARNIC 429 interface (2No)

ARINC429 protocol is not supported by our QorIQ family networking processors.

External third-party controller will be required (if any). Alternatively, you can consider a device from Automotive or Industrial product segments, these devices have “eTPU” block, which may be used to implement ARINC429.

 

2)CAN interface (2No)

CAN interface is not supported in P5020 processor, please consider another device – for example P1010 or LS1021A.

 

3)RS422 interface(2No)

RS422 is “electrical” standard, typically UART with RS422 transceivers is used. Yes, UART is supported.

 

Have a great day,

Alexander
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信