P4080 Chip Errata

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 Chip Errata

Jump to solution
1,123 Views
minghu_du
Contributor III

The P4080 Chip Errata Revision R was published in 2013, does anyone know if there is a later P4080 chip errata than the revision R?

Tags (2)
1 Solution
1,035 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

It is the last avaialble revision of  P4080 Chip Errata. 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
1,036 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

It is the last avaialble revision of  P4080 Chip Errata. 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------