P3041 SATA registers base address.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P3041 SATA registers base address.

ソリューションへジャンプ
690件の閲覧回数
dshard
Contributor I

Hello!

Can u help me find P3041 SATA registers base adress?

タグ(2)
0 件の賞賛
1 解決策
579件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The local address map location of SATA register block is controlled by the configuration, control, and status registers base address register (CCSRBAR) The default value for CCSRBAR is 0_FE00_0000h, but it can be changed (typically it may be changed on boot). In the CCSR Block the SATA1 takes 0x22_0000-0x22_0FFF, while SATA 2 takes 0x22_1000-0x22_1FFF. I.e. base address is
CCSRBAR +0x22_0000 for SATA1 and
CCSRBAR +0x22_1000 for SATA2.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
580件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The local address map location of SATA register block is controlled by the configuration, control, and status registers base address register (CCSRBAR) The default value for CCSRBAR is 0_FE00_0000h, but it can be changed (typically it may be changed on boot). In the CCSR Block the SATA1 takes 0x22_0000-0x22_0FFF, while SATA 2 takes 0x22_1000-0x22_1FFF. I.e. base address is
CCSRBAR +0x22_0000 for SATA1 and
CCSRBAR +0x22_1000 for SATA2.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛