P2041RDB can't boot from RAM with hypervisor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2041RDB can't boot from RAM with hypervisor

Jump to solution
1,178 Views
sophiebonnouvri
Contributor II

Hi,

I'm working with an P2041RDB, I can boot from NOR with hypervisor without pb.

Now I try to boot from RAM.

     - start U-boot

     - tftp HV , HV FDT, board FDT, kernel , rootfs in RAM

   

The Hypervisor start, get FDT but the kernel don't start ...

I check in RAM guest memory at @0  and @0x01300000 => It's fill with 0x00 => no data

In HV FDT tree ,I have :

fdt list /part1 guest-image

guest-image = <0x00000000 0x22a72866 0x00000000 0x00000000 0x00000000 0x00700000>

fdt list /part1 linux-rootfs

linux-rootfs = <0x00000000 0x2006a066 0x00000000 0x01300000 0x00000000 0x05d00000>

The @ of the kernel /rootfs are good (0x22a72866 0x2006a066), I have check with imi cmd in U-boot

U-boot/kernel etc are from SDK 1.5

It's seems like the address is'nt pass correctly to the hypervisor, but in the log It the good one.

If somebody have an idea, thanks

Sophie

LOG :

bootm $hv_addr - $boardfdt_addr (bootm 20003a66 - 22a6a266)

WARNING: adjusting available memory to 30000000

## Booting kernel from Legacy Image at 20003a66 ...

   Image Name:

   Image Type:   PowerPC Linux Kernel Image (uncompressed)

   Data Size:    418584 Bytes = 408.8 KiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 22a6a266

   Booting using the fdt blob at 0x22a6a266

   Loading Kernel Image ... OK

OK

   Loading Device Tree to 03fe4000, end 03fff37f ... OK

ERROR: could not find compatible node fsl-usb2-mph or fsl-usb2-dr: FDT_ERR_NOTFOUND.

[0] =======================================

[0] Freescale Hypervisor 3.0-001

[0] Hypervisor command line: config-addr=0x20000666 console=ttyS0,115200

[0] malloc_init: using 15799 KiB at 0xf1092480 - 0xf1ffffff

[0] dt_read_aliases: Alias pci0 points to non-existent /pcie@ffe200000

[0] dt_read_aliases: Alias pci2 points to non-existent /pcie@ffe202000

[0] loading binary image from 0x2006a066 to 0x1300000

[0] loading binary image from 0x22a72866 to 0

[0] branching to guest p1-linux, 1 cpus

[0] starting primary guest in supervisor mode

HV>

Tags (2)
0 Kudos
1 Solution
669 Views
sophiebonnouvri
Contributor II

In the dts file the parameter zero-pma  :"If present causes the PMA to be initialized to zeros during the cold boot of a system."

You have to remove it if you want to boot Hypervisor with image in RAM.

View solution in original post

0 Kudos
3 Replies
669 Views
sophiebonnouvri
Contributor II

Hi,

Does anybody know if the Hypervisor clear the RAM before loading uImage ?

sophie

0 Kudos
670 Views
sophiebonnouvri
Contributor II

In the dts file the parameter zero-pma  :"If present causes the PMA to be initialized to zeros during the cold boot of a system."

You have to remove it if you want to boot Hypervisor with image in RAM.

0 Kudos
669 Views
amittomar
NXP Employee
NXP Employee

Hi Sophie

I am facing issue ,booting the Hypervisor from RAM.

Would you please let me know the exact RAM addresses you used while tftp HV , HV FDT, board FDT, kernel , rootfs in RAM?

Did you configure any specific boot args at U-boot?

Also,did you use same kernel/rootfs image for guest and host?

Thanks

Amit.

0 Kudos