P2020's memory updating from DDR2 to DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020's memory updating from DDR2 to DDR3

646 Views
billy_huan
Contributor I

Hi NXP:

Our new design should update P2020's memory from DDR2 to DDR3.

But there is no ddr reset pin of P2020 mmu.

So, how can I deal with the ddr reset logic without CPLD?

Can connect the pin to Power on reset directly?

Billy Huan

B.R.

0 Kudos
2 Replies

504 Views
billy_huan
Contributor I

I got it.

Thanks a lot.

0 Kudos

504 Views
ufedor
NXP Employee
NXP Employee

As  DDR3 reset it is possible to use a copy of the reset signal going to the P2020's HRESET input.

0 Kudos