P2020 PTP EVENT POLLING

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2020 PTP EVENT POLLING

417 Views
mohitduggal
Contributor II

I was using P2020rdb board . I have written  program to monitor ptp timer event register for input trigger pulse. 1PPS input is given to that board and whenever rising edge comes an event is generated in timer event register. the event is monitored and GPIO is made high based on that input pulse for 20 microseconds. But i have getting a variable delay of 4 micorsecond to 6 microseconds in it. even after changing scheduler to RR or FIFO the delay remains the same. Could someone help in reducing that delay , please find below the code snapshot

extts_reg_l = *TMR_ETTS1_L;
 
    while (1) {
    if(((extts_reg_l - *TMR_ETTS1_L) != 0) )
    
    {
        
         *GPIO_DAT_REG |= 0x200000;           
        //1830 = 20 usec        
        
         for(i=0;i<(1830);i++)
         {
           ;
         }
                extts_Reg64 = (UINT64) *TMR_ETTS1_H;
                extts_Reg64  = (uint64_t)(extts_Reg64 << 32);
                tmp_reg = *TMR_ETTS1_L;
                extts_Reg64 |= (UINT64) tmp_reg;
            
                extts_ts = (uint64_t)extts_Reg64;
                
        //extts_offset = extts_ts % (NS_PER_SEC);
        
        extts_offset = extts_ts % (NS_PER_SEC);
                         
        if (extts_offset > NS_PER_SEC / 2 )
            extts_offset -= (NS_PER_SEC);
            
            extts_reg_l = *TMR_ETTS1_L;
            
        *GPIO_DAT_REG &= 0xFFDFFFFF;//low
        
        
        //if(servo_active)
        //{    
                
            do_servo(&servo, FD_TO_CLOCKID(phc_fd), extts_offset, extts_ts, kp, ki);
        //}
        //show_servo(stdout, "extts", extts_offset, extts_ts);
    }

 

0 Kudos
0 Replies