Hello!
History of analisys of problem is here https://community.freescale.com/message/653136. Because problem is very important, I create new question thread.
I find bug in P1020 eTSEC controller.
Problem: eTSEC put to RxBDs ring previous packet, not last received.
Method that activate the problem: We connect from one PC to device 2 way. 1. Ping. 2. Cyclic download files from device to PC. We restart device every 20-30 min, and problem is activated several times during one day.
Using software: linux QorIQ SDK 1.9
I add debug to gianfar, and see that ETSEC put to RxBDs ring only previous packet, not last received. I send to device various length packets, log bdp->lstatus (in gfar_clean_rx_ring()) for current and next BDP and see this behaviour very well.
Problem occurs when eTSEC packet parser is enabled (RCTRL[PRSDEP]=0x11). When eTSEC packet parser is disabled (RCTRL[PRSDEP]=0x0)? problem not occurs. Problem not depend on filer. Problem occurs when filer is enabled (RCTRL[FILEN]=1) or disabled (RCTRL[FILEN]=0).
Registers state after problem is occured.
root@p1020rdb:~# ethtool -d eth0
Offset Values
------ ------
0x0000: 01 24 02 00 00 ee 00 f0 00 00 00 00 00 00 00 00
0x0010: 00 00 00 00 f1 31 00 83 00 00 00 00 00 00 00 00
0x0020: 00 00 10 0c 00 00 00 00 00 00 00 04 00 00 00 c3
0x0030: 00 00 00 1f 00 00 00 00 00 00 00 00 00 00 00 00
0x0040: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0050: 00 00 00 80 00 00 00 c0 00 00 00 40 00 00 00 80
0x0060: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0070: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0080: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 01 00
0x0090: 00 00 00 00 00 00 00 00 00 00 00 40 00 00 00 80
0x00a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x00f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0100: 00 00 60 02 80 00 80 00 81 00 00 00 00 00 00 00
0x0110: 82 00 00 15 00 00 80 00 00 00 00 00 00 00 00 00
0x0120: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0130: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0140: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0150: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0160: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0170: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0180: 00 00 00 00 17 45 02 60 00 00 00 00 00 00 00 00
0x0190: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x01f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0200: 00 00 00 00 17 45 00 00 00 00 00 00 00 00 00 00
0x0210: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0220: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0230: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0240: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0250: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0260: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0270: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0280: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0290: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x02f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0300: 00 08 77 c2 02 00 00 80 00 00 00 00 00 00 00 00
0x0310: 00 00 00 00 00 80 00 80 04 10 41 00 00 00 00 00
0x0320: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0330: 00 00 00 00 00 00 00 e6 00 00 00 60 ff ff ff ff
0x0340: 00 00 06 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0350: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0360: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0370: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0380: 00 00 00 00 17 45 0b 08 00 00 00 00 00 00 00 00
0x0390: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x03a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x03b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x03c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x03d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x03e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x03f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0400: 00 00 00 00 17 45 08 00 00 00 00 00 00 00 00 00
0x0410: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0420: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0430: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0440: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0450: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0460: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0470: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0480: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0490: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x04a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x04b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x04c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x04d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x04e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x04f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0500: 00 00 00 0f 00 00 71 05 40 60 50 60 00 a1 f0 37
0x0510: 00 00 06 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0520: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0530: 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00
0x0540: 00 40 04 c5 1b 00 00 00 01 00 00 5e 00 01 00 00
0x0550: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0560: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0570: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0580: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0590: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x05a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x05b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x05c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x05d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x05e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x05f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0600: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0610: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0620: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0630: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0640: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0650: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0660: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0670: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0680: 00 01 5e ac 00 00 d2 9d 00 00 19 7c 00 00 0f 17
0x0690: 00 00 12 af 00 03 64 a8 00 00 00 00 00 90 09 7c
0x06a0: 00 02 04 33 00 00 01 42 00 00 00 57 00 00 00 8f
0x06b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x06c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x06d0: 00 00 00 00 00 00 11 be 00 00 00 00 00 00 00 5e
0x06e0: 10 93 18 a5 00 03 de be 00 00 00 00 00 00 00 00
0x06f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0700: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0710: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0720: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0730: 00 00 00 00 00 00 00 00 fe 03 ff ff 00 0f ff fd
0x0740: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0750: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0760: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0770: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0780: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0790: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x07a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x07b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x07c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x07d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x07e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x07f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0800: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0810: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0820: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0830: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0840: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0850: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0860: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0870: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0880: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0890: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x08a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x08b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x08c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x08d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x08e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x08f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0900: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0910: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0920: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0930: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0940: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0950: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0960: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0970: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0980: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0990: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x09a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x09b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x09c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x09d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x09e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x09f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a00: 00 00 00 c0 00 00 00 00 00 00 00 00 00 00 00 00
0x0a10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0a90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0aa0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ab0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ac0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ad0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ae0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0af0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0b90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ba0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0bb0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0bc0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0bd0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0be0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0bf0: 00 00 00 00 00 00 00 00 00 00 48 c0 00 60 00 00
0x0c00: 10 00 01 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c40: 00 00 00 00 17 45 08 00 00 00 00 00 00 00 00 00
0x0c50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0c90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ca0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0cb0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0cc0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0cd0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ce0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0cf0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0d90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0da0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0db0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0dc0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0dd0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0de0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0df0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e00: 00 01 00 01 00 00 00 00 00 00 00 00 00 00 00 00
0x0e10: 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00
0x0e20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0e90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ea0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0eb0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ec0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ed0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ee0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ef0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f10: 82 00 00 15 00 00 00 00 00 00 00 00 00 00 00 00
0x0f20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0f90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0fa0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0fb0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0fc0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0fd0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0fe0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
0x0ff0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
Original Attachment has been moved to: radius_oe.dts.zip
Original Attachment has been moved to: 1.pcap.zip
Original Attachment has been moved to: radius_defconfig.zip
The issue you are describing doesn't look typical. It's analysis and discussion it is likely
to require long time, exchanging large amounts of information and possibly NDA documentation and/or
details of your hardware design which is not appropriate for a public forum. For this reason, may I suggest that you
create a Support Case for it?
Details on how to create Support Cases can be found here:
https://community.nxp.com/docs/DOC-329745
Regards,
Platon