P1020 by PCIE and exchange chip BCM56450 mapping a momery,have a problem for read and write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1020 by PCIE and exchange chip BCM56450 mapping a momery,have a problem for read and write

455 Views
damonmeng
Contributor II

1. P1020 by PCIE and exchange chip BCM56450 mapping a momery, about read and write,reverse order is right, Positive sequence is wrong,such as writing 5,4,3,2,1,that is right, writing 1, 2, 3, 4, 5 is wrong, please if have a register set can be positive sequence writing?
2. Is there a register can set the big end and small end?
 
There is no such Settings, whether need to change the software?

Thanks!

0 Kudos
1 Reply

347 Views
bpe
NXP Employee
NXP Employee

PCIe is inherently little endian. See P1020RM, Section 14.12.1.2
for advanced discussion.

0 Kudos