P1010RDB TWBE NAND parameter

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1010RDB TWBE NAND parameter

1,008 次查看
renaud
Contributor IV

I see that in the U-Boot support package for the P1010RDB-PB that the NAND MT29F16G08ABABAWP is used.

I noticed that the parameter TWBEis set to 0x39 = 57. Assuming the IFC clock is 100 MHz or 10ns. That would

set TWBE to 570ns. That seems to be 5 times above the maximum specified in the NAND timing (tWB) that can be from

200 to 100 ns depending on the mode. Is there a reason for that?

Cheers,

Renaud

0 项奖励
回复
1 回复

926 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Renaud,

The IFC NAND TWBE parameter is calculated according to NAND flash parameters, please refer to the related NAND Flash datasheet.

TWBE = ROUNDUP((twb-twh)*(NAND flash  Clock Frequency)/1000)

twb is 200ns

twh is 30ns

clock frequency is 330MHz

TWBE = ROUNDUP((200-30)*330/1000)=57


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复