P1010RDB TWBE NAND parameter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010RDB TWBE NAND parameter

1,005 Views
renaud
Contributor IV

I see that in the U-Boot support package for the P1010RDB-PB that the NAND MT29F16G08ABABAWP is used.

I noticed that the parameter TWBEis set to 0x39 = 57. Assuming the IFC clock is 100 MHz or 10ns. That would

set TWBE to 570ns. That seems to be 5 times above the maximum specified in the NAND timing (tWB) that can be from

200 to 100 ns depending on the mode. Is there a reason for that?

Cheers,

Renaud

0 Kudos
Reply
1 Reply

923 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Renaud,

The IFC NAND TWBE parameter is calculated according to NAND flash parameters, please refer to the related NAND Flash datasheet.

TWBE = ROUNDUP((twb-twh)*(NAND flash  Clock Frequency)/1000)

twb is 200ns

twh is 30ns

clock frequency is 330MHz

TWBE = ROUNDUP((200-30)*330/1000)=57


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply