P1010RDB_PA vs P1010RDB_PB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1010RDB_PA vs P1010RDB_PB

696 Views
fabricedecrop
Contributor I

Hi,

I'm using hardware base on P1010RDB. I was wondering what were the differences between P1010RDB revision A and revision B ? Or, do you know where I can find this information ?

On my board, there is a sticker with "P1010-RDB" written on it. I'm assuming that's a "revision A" board. Is it correct ?

Thanks in advance,

Regards,

Fabrice DECROP

Tags (2)
0 Kudos
Reply
1 Reply

515 Views
r8070z
NXP Employee
NXP Employee


Have a great day,


The P1010RDB-PA has the P1010 rev. 1.0 only. The P1010RDB-PA comes in plastic casing whereas the P1010RDB-PB comes in metal casing. The P1010RDB-PA has two USB ports whereas PB has only one. P1010RDB-PA has 32MB NAND, P1010RDB-PB has 2GB NAND

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply